2023-10-29 10:01 AM - edited 2023-10-29 10:03 AM
I have used the Cube examples "Thread_FTD_Coap_Multicast" and "Thread_SED_Coap_FreeRTOS" and I was able to receive CoAP multicast from SED to the thread leader however I am not able to send messages to the SED in any way at all when I pressed SW1 on the Nucleo board.
I also tried the Thread CLI as a leader with the following commands:
panid 0x2222
channel 12
networkkey 00112233445566778899aabbccddeeff
ifconfig up
thread start
coap start
And I saw that the Thread CLI was in Leader state and SED was connected to the thread CLI but I was not getting any CoAP messages from SED and I was not able to send any messages to SED either through CoAP (GET, PUT, POST) (CON/NON-CON).
I would appreciate any pointers on how to achieve the Leader->SED communication through CoAP, or if any modifications necessary as I am quite new to OT devel.
Thanks in advance
Some boilerplate info:
STM32CubeIDE V1.13.2
STM32CubeWB V1.17.3
Thread SED:
P-NucleoWB55 // STM32WB55RG
M0 Copro FW: stm32wb5x_Thread_MTD_fw.bin V1.17.1
CFG_FULL_LOW_POWER set to DISABLED
Thread Leader:
P-NucleoWB55 // STM32WB55RG
M0 Copro FW: stm32wb5x_Thread_FTD_fw.bin V1.17.1
Solved! Go to Solution.
2023-10-31 12:48 AM
Thank you for the warm welcome @STTwo-32 !
I have already tried the example you suggested (FTD Multicast) on two boards. it works as expected.
But as I am developing a battery powered device (which will involve a Thread SED), I wish to know how to receive CoAP on the SED.
It would be amazing if you could help me out on how to achieve it.
Regarding the Thread CLI, I was able to fix it by creating the resource manually after starting CoAP with the command:
coap resource light
This fixed the issue and I was able to receive the CoAP from SED->Leader. I am posting this as it may be useful for someone in the future looking for the fix.
2023-10-31 12:21 AM
Hello @shreyask21 and welcome to the ST Community
As I understand, you are looking to have a bidirectional communication between 2 STM32WB55RG_Nucleo in a thread network. For that, I suggest you use the Thread_FTD_Coap_Multicast example on both boards.
best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-31 12:48 AM
Thank you for the warm welcome @STTwo-32 !
I have already tried the example you suggested (FTD Multicast) on two boards. it works as expected.
But as I am developing a battery powered device (which will involve a Thread SED), I wish to know how to receive CoAP on the SED.
It would be amazing if you could help me out on how to achieve it.
Regarding the Thread CLI, I was able to fix it by creating the resource manually after starting CoAP with the command:
coap resource light
This fixed the issue and I was able to receive the CoAP from SED->Leader. I am posting this as it may be useful for someone in the future looking for the fix.