cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO WL55JC1 P2P(GW) Support and LoRaWAN Node Capacity

Deep23
Associate

Hello,

We are currently working with the NUCLEO-WL55JC1 board for LoRa communication and have a few technical queries.

1. STM32WL as Gateway / P2P Receiver
We are planning to use two NUCLEO-WL55JC1 boards, where:

  • One board will act as a LoRa end node

  • The other board will act as a gateway or P2P receiver

  • Is there any gateway or P2P receiver firmware example available in the STM32WL SDK for the NUCLEO-WL55JC1 board?

2. LoRaWAN Gateway Capacity

We would also like to understand the theoretical number of end nodes that can be supported by a single LoRaWAN gateway under the following conditions:

 

  • Payload size: 16 bytes

  • Spreading Factor: SF10

  • Uplink transmission interval: 1 hour per nodeAny calculation method, reference document, or guideline from your side would be very helpful.

 

0 REPLIES 0