2025-07-12 4:22 AM
Hello ,
I'm trying to flash in the NUCLEO WBA52CG the basic code example available in STM32CubeIDE. I use version 1.19 with Windows. It was originally version 1.17 and was updated in 1.19.
No issue to generate the code or build it. I then connected the NUCLEO WBA52CG and wanted to flash in the board.
I got the failure message "No device found on target."
Can anyone help me ?
I added below a pictures of the connected board. Some leds ( green and red ones) are blinking but I don't know if it's OK or not
Thanks in advance
Regards
Serge
Solved! Go to Solution.
2025-07-17 6:25 AM
Hello
After uninstalling STM32CubeIDE version 1.17 updated in version 1.19 and installing version 1.19 directly from the scratch it’s working fine.
Thank you for your help
Regards,
Serge
2025-07-12 5:03 AM
Hello @Serge1
does it work fine with the STM32CubeProg V2.20.0 (try different mode such as the under reset, normal…).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-14 9:56 AM
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Christian
2025-07-17 6:25 AM
Hello
After uninstalling STM32CubeIDE version 1.17 updated in version 1.19 and installing version 1.19 directly from the scratch it’s working fine.
Thank you for your help
Regards,
Serge