cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo STM32WL55 Running LoRaWAN AT Slave - Why no Lora transmission?

kiwironnie
Associate III

Have built the (single core) LoRaWAN AT Slave example from STM32Cube_FW_WL_V1.0.0, which has been flashed to a new Nucleo STM32WL55 board (straight out of the package). No apparent problems building and flashing. Configured for AS923 region.

Running an OTAA Join command the terminal returns:

AT+JOIN=1

35s069:TX on freq 923400000 Hz at DR 2

OK

35s461:MAC txDone

40s447:RX_1 on freq 923400000 Hz at DR 2

40s523:MAC rxTimeOut

41s447:RX_2 on freq 923200000 Hz at DR 2

41s523:MAC rxTimeOut

+EVT:JOIN FAILED

Looks ok but problem is that the radio isn't transmitting at all, as checked with a spectrum analyser (which sees output from other LoRaWAN boards running that frequency band).

Could be a simple configuration problem, but everything looks ok.

Suggestions would be welcome?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
kiwironnie
Associate III

Oh Oh!

Answer to this question is that I have the low frequency version of the Nucleo board!! It does transmit but output is of course very weak at around 923MHz.

Darn. Have just ordered the correct board.

View solution in original post

1 REPLY 1
kiwironnie
Associate III

Oh Oh!

Answer to this question is that I have the low frequency version of the Nucleo board!! It does transmit but output is of course very weak at around 923MHz.

Darn. Have just ordered the correct board.