2022-06-01 3:11 AM
Hello,
From 1.13.0 to 1.13.3, the command ACI_HAL_TONE_START was removed (get Unknown command return). The release note indicates that some HCI commands were removed not ACI commands.
Is it an error or should we prepare to move to the full extended stack to get this API again ?
We are using it during industrialization process to check the radio frequency and power.
Is it planned to update the API spec (AN5270) to indicate which API are not present in the full stack ?
BR
Anthony
Solved! Go to Solution.
2022-06-03 12:58 AM
Hello,
To use extended binaries, it is necessary to adapt the scatter file in the BLE applications, you can look this post which I explain the modification to do in the scatter file:
Thanks to your remarks, the ACI_HAL_TONE_START and ACI_HAL_TONE_STOP commands will be available in BLE Full and Light stack in the next release v1.14.0 available soon.
Best Regards
2022-06-02 2:07 AM
Hello,
Indeed the ACI_HAL_TONE_START command was removed in BLE Full stack v1.13.3. In order to use this command, you can use the BLE Full stack extended or the BLE HCI Layer stack. The AN5270 and STM32WB_BLE_Wireless_Interface.html documentation will be updated soon. A wiki page is also under redaction to give more detail on each feature supported depending of stack used.
Best Regards
2022-06-02 2:34 AM
Hello,
I tried to update to the full extended but I found 2 issues:
From my point of view removing API from the "full" stack breaks the API compatibility and is bad idea.
BR
2022-06-03 12:58 AM
Hello,
To use extended binaries, it is necessary to adapt the scatter file in the BLE applications, you can look this post which I explain the modification to do in the scatter file:
Thanks to your remarks, the ACI_HAL_TONE_START and ACI_HAL_TONE_STOP commands will be available in BLE Full and Light stack in the next release v1.14.0 available soon.
Best Regards
2022-06-03 4:57 AM
Hello,
Thank you. I will stay on 1.13.0 until 1.14.0 is available.
BR
2022-07-07 6:31 AM
Hello,
STM32CubeWB package v1.14.0 is now available.
Best Regards