2024-07-25 10:02 PM
1. Does these two parts have same SubGHz radio?
2. NUCLEO-WL55JC is dual core. Is it correct that most examples use single core? If so, do they use the M0 or M4 core? Does the examples applicable to STM32WLE5JC? Does the HAL layer make the C code applicable to both parts?
3. Nucleo has board support pack (BSP). What do they contain? Only simple LED and Switch port/pin pair or something more complex. We are using the bare STM32E5JC chip, not a board, so no BSP.
Many thanks
2024-08-29 8:11 AM
Hello @David_
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.