cancel
Showing results for 
Search instead for 
Did you mean: 

Is after pressing button to "Start Wireless Stack" in STM32CubeProgrammer supposed to load something in to flash starting at 0x08000000

tj.1
Associate

I am using STM32CubeProgrammer trying to correctly start BLE stack.

Problem is that when I press "Start Wireless Stack" inside the program it loads some data into flash between addresses 0x08000000 - 0x08001700 but the space on a STM32WB50CG from address 0x08000000 to 0x08020000 is supposed to be reserved for user programs, so a part of mine gets overridden.

I am fairly new to ARM development, so I just want to know, if after pressing button to "Start Wireless Stack" is supposed to load something in to flash starting at 0x08000000 or am I doing something wrong. Any suggestions what to check?

Overall MPU setup was done by official STM tutorial, but BLE doesn't show up as someone in comment section also pointed out.

https://www.youtube.com/watch?v=i10X4Blr8ns

08:37:26 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
  08:37:26 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
  08:37:26 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
  08:37:26 : Warning: Option Bytes are unchanged, Data won't be downloaded
  08:37:26 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 
  08:37:26 : Memory Programming ...
  08:37:26 : Opening and parsing file: 0x495_FUS_Operator.bin
  08:37:26 :   File          : 0x495_FUS_Operator.bin
  08:37:26 :   Size          : 8 KBytes
  08:37:26 :   Address       : 0x08000000 
  08:37:26 : Erasing memory corresponding to segment 0:
  08:37:26 : Erasing internal memory sectors [0 1]
  08:37:27 : Download in Progress:
  08:37:27 : File download complete
  08:37:27 : Time elapsed during download operation: 00:00:00.285
  08:37:27 : Application is running, Please Hold on...
  08:37:28 : Reconnecting...
  08:37:28 : Reconnected !
  08:37:29 : FusStartWS activated successfully
  08:37:29 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
  08:37:29 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
  08:37:29 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
  08:37:29 : Warning: Option Bytes are unchanged, Data won't be downloaded
  08:37:29 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 
  08:37:29 : Memory Programming ...
  08:37:29 : Opening and parsing file: 0x495_FUS_Operator.bin
  08:37:29 :   File          : 0x495_FUS_Operator.bin
  08:37:29 :   Size          : 8 KBytes
  08:37:29 :   Address       : 0x08000000 
  08:37:29 : Erasing memory corresponding to segment 0:
  08:37:29 : Erasing internal memory sectors [0 1]
  08:37:29 : Download in Progress:
  08:37:29 : File download complete
  08:37:29 : Time elapsed during download operation: 00:00:00.281
  08:37:29 : Application is running, Please Hold on...
  08:37:30 : Reconnecting...
  08:37:30 : Reconnected !
  08:37:31 : FusStartWS activated successfully
  08:37:31 : Start Wireless Stack command execution finished with success

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Remy ISSALYS
ST Employee

Hello,

Indeed, when you press "Start Wireless Stack" , STM32CubeProgrammer loads FUS operator into the flash at 0x08000000 in the applicative part to be able to start wireless stack.

Best Regards

davidnguyen2023
Associate

Hi,

 

Can I use the firmware to "Start Wireless Stack" instead using STM32CubeProgrammer ?

 

David