2023-06-01 7:17 AM
Hello everyone, I am trying to make a project with pingpong application. I am trying to add some sensors and fft algorithm in ping pong example.
In normally I can use my FFT algorithm with ADC-DMA in while loop().
HAL_ADC_Start_DMA(&hadc, (uint32_t*) rxBuf, 8192);
arm_rfft_fast_init_f32 (&fft_handler, 2048);
while (1)
{
int fft_in_ptr = 0;
if (callback_state == 1)
{
for (int i=0; i<8192; i=i+4)
{
fft_in_buf[fft_in_ptr] = (float) ((int) (rxBuf[i]<<16)|rxBuf[i+1]);
fft_in_buf[fft_in_ptr] += (float) ((int) (rxBuf[i+2]<<16)|rxBuf[i+3]);
fft_in_ptr++;
}
DoFFT();
}
if (callback_state == 2)
{
for (int i=0; i<8192; i=i+4)
{
fft_in_buf[fft_in_ptr] = (float) ((int) (rxBuf[i]<<16)|rxBuf[i+1]);
fft_in_buf[fft_in_ptr] += (float) ((int) (rxBuf[i+2]<<16)|rxBuf[i+3]);
fft_in_ptr++;
}
DoFFT();
}
}
}
void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc)
{
callback_state = 1;
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
callback_state = 2;
}I can get frequencies of tone correctly. As you can see, I am using while loop for this. I am confused how can I use this code in ping-pong or other application. What is the best way to use this on ping-pong or similar application?
Should I set another sequencer for it? (but this will block cpu I guess)
So I really need advice when adding this to these application such as ping-pong.