cancel
Showing results for 
Search instead for 
Did you mean: 

Get CRC Error after transmit

KimiHu
Associate

Hi all,

My application is showing below

Device(NUCLEO-WL55JC1 EVM) send data to Gateway --> wait 100msec --> enter receive to wait data from gateway. In my test, If data from gateway more then device. The device report CRC Error to application layer.

I reproduce similar problem with (sample code)

1. Import SubGHz_Phy_Per and build it as TX side

2. Use attachment as RX side

3. IF data data length less then 64. I will get IRQ_CRC_Error and OnRxDone at the same time

  

1 REPLY 1
STTwo-32
ST Employee

Hello @KimiHu 

I suggest you to debug the RX project. this will help you locating the error source.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.