cancel
Showing results for 
Search instead for 
Did you mean: 

Expansion Board with Quad SPI NOR FLASH

DavePfz
Associate III

Are there any expansion boards with Quad SPI NOR Flash chips? I am interested in using it with a NUCLEO-WB55RG board.Preferably it should use the Macronix 25L6433FM2I-08G chip, but that is not a hard requirement. This chip is found on the X-NUCLEO-GFX01M2 board, but it is implemented as a standard single SPI interface.

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @DavePfz ,

I did not find an expansion board for the Nucleo-WB55RG that includes a Quad-SPI NOR flash memory. You can use a Discovery board, such as the STM32WB5MM-DK board, which supports Quad-SPI mode and embeds a 128-Mbit Quad-SPI NOR Flash Memory.
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @DavePfz ,

I did not find an expansion board for the Nucleo-WB55RG that includes a Quad-SPI NOR flash memory. You can use a Discovery board, such as the STM32WB5MM-DK board, which supports Quad-SPI mode and embeds a 128-Mbit Quad-SPI NOR Flash Memory.
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
DavePfz
Associate III

Thanks for looking into this. I came to the same conclusion. Although the STM32WB5MM-DK was not exactly what I was looking for it did give me the information I needed.

Thanks