2023-07-25 5:59 AM
Hi Support, we want to be able to generate a 2.4GHz Bluetooth carrier wave to test our hardware.
Is there a sample project or a sample .hex file I could use to do this.
Also pointing me to the correct documentation to achieve this would be greatly appreciated.
Thanks
2023-07-31 6:50 AM
Hello,
You can used BLE_TransparentMode example with stm32wb5x_BLE_Stack_full_extended_fw.bin binary available in STM32CubeWB package. Using STM32CubeMonitor RF tool, you can send aci_hal_tone_start command to start a carrier frequency, i.e. a tone, on a specific channel. You can refer to the following documentation for more detail on this command, see STM32WB_BLE_Wireless_Interface.html in STM32Cube_FW_WB_V1.17.0\Middlewares\ST\STM32_WPAN\ble\core\doc.
Best Regards