Erasing of flash in STM32WB BLE OTA example not working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-09-23 4:03 AM
I have loaded BLE OTA example (v1.13.1) to my STM32WB50CG. User application starts on default set address 0x08007000. Problem is when I send a BLE command to OTA Reboot characteristic (to load into OTA, first sector + how many to delete) from my Android app to the STM the flash never deletes. I've been debuging the OTA STM example code but everything returns status OK except flash doesn't actually erase. After this command is sent, I disconnect the phone from the STM board.
If I manually delete flash via STMCube Programmer, BLE OTA example then completely works as intended.
Any idea what could be the cause?
- Labels:
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-10-05 2:12 AM
Hello,
Do you see the same behavior when using BLE_HeartRate_ota or BLE_p2pServer_ota examples ?
Best Regards