cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STM32WBA65 support the channel sounding feature of BLE 6.0?

TechUmNu
Associate

The product page and datasheet only mention BLE Core 6.0 but don't call out channel sounding support explicitly like other BLE features. Is it actually supported?

1 ACCEPTED SOLUTION

Accepted Solutions
Petr DAVID
ST Employee

Yes, the STM32WBA6 is Bluetooth LE 6.0 certified. However, it does not support Channel Sounding.
Please note that Channel Sounding is not only a software feature; it also requires specific hardware/IP support in the device architecture, which is not available on STM32WBA6.

Kind regards,
Petr

View solution in original post

4 REPLIES 4
Petr DAVID
ST Employee

Yes, the STM32WBA6 is Bluetooth LE 6.0 certified. However, it does not support Channel Sounding.
Please note that Channel Sounding is not only a software feature; it also requires specific hardware/IP support in the device architecture, which is not available on STM32WBA6.

Kind regards,
Petr

Thank you for the fast reply Petr!

Is channel sounding something that you expect ST to support with a different device in the future? 

Yes, there will be a device with channel sounding in the future - stay tuned!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @TechUmNu and welcome to the Community,

For projects requiring channel sounding feature, you can also consider alternative or future platforms such as the STM32WBA2 lines, which are planned to address this use case.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen