2025-04-28 12:16 AM
Got this issue on entering sleep.
I set my advertising to 1 second, and do not touch it after.
Before sleep, all was good, I was advertising every ~1 second
but when I enter sleep I notice it jumps to 1 or 2 ms.. very fast, and not so power consuming.
I didn't test with power testing tool, to validate the peaks, but only via the phone app.
Wonder what might be causing this?? Do I accidently shutdown some peripheral important for BLE?
Solved! Go to Solution.
2025-06-04 7:20 AM
I followed the PLL example I think BLE_HearRate_PLL and that helped.
One of the clocks was misconfigured.
2025-04-30 4:21 AM
Hello,
can you please describe the issue more in detail? Can you show any waveform?
Also, if you could share the steps when you're testing it, so I could reproduce it on my side.
Thank you.
Best regards,
ST support
2025-05-11 12:03 AM
We are currently trying to get our hands on a better sniffing tool, but this might take some time..
Meanwhile, did manage to improve it slightly by following the free rtos example with ble.
BTW, I am on stack 21 .
Now, I see a drop from 1 sec ( initial pre sleep setting ) to around 200-250 ms during sleep.
Any idea to why do I get this drop? Any debug I can add to BLE stack? Anything you know of that might be causing this ?
I did follow the example as much as possible. HAL, RTC, CLOCKS.. ( FreeRTOS BleHeartRate)
We use a slightly different operating system, a CMSIS one.
Do you guys have a CMSIS RTOS sleep example?
2025-05-12 7:14 AM
Hello,
which board do you use? Is it a custom board? You can enable debug traces in the app_conf.h file.
Can you please share the measurement? Thank you.
Unfortunately, there is no CMSIS RTOS sleep example in the WB package.
Best regards,
ST support
2025-05-12 11:39 AM - edited 2025-05-12 11:40 AM
As soon as we hit EnterLowPower() , out advertising goes crazy ( 1- 2 ms )
This pretty sure is caused because we use PLL's in SystemClock_Config .
They are used also for our :ADC , RTC.
(Although that's not the config you guys use in your example)
After turning PLL off , no issue !
BUT WHY?
and is there any way we don't have to make grand changes in our clocks to fix this?
.
2025-06-04 7:20 AM
I followed the PLL example I think BLE_HearRate_PLL and that helped.
One of the clocks was misconfigured.