cancel
Showing results for 
Search instead for 
Did you mean: 

BLE lost packets in high througput app

aarnaizz
Associate

Hello!

I am having trouble with lost BLE packets in my system:

- TX: STM32WB15CC

- RX: nRF52840

I have tried so many different things to patch this, but I continue struggleling. For my app, I get a 247B frame ready to be sent every 3ms, so I need a high througput for BLE. However, theoretically I should be possible to get around 10m or more without losses, whereas I get roughly to 4m.

There seem to be two main problems:

  • The first one takes place in the link and the environment. As packets do not reach their destination succesfully, I suspect there has to be interferences or some kind of distorion that gets the packets lost in the air.
  • The second one is around the BLE queues in the transmitter. I believe there could be overflow in the buffers or some timeout running out when failing to retransmit the packets that are lost in the link.

However, as I do not have such a great experience, I do not know how to analyse what is exactly happening with the queues and how much memory are they able to store without losses. Futhermore, I know there is a queue implemented in my main system that is able to store 22 BLE packets in case there is a need of retransmission. But, is this the only buffer that works in the STM32? I am aware of another queue related to the secondary cortex, but I do not know how does it work. Could someone help me with it?

At the same time, this system was provided to me by another developer, so I do not quite control everything about it, as I already demonstrated.

This is the whole summary of the project, but there are lots of details that I would be so happy to share if they were helpful for solving the packet losses problems.

 

Thank you in advance,

Álvaro Arnáiz.

 

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @aarnaizz 

I suggest you perform some tests using two STM32WB Nucleo boards for TX and RX. It may improve your system performance.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.