cancel
Showing results for 
Search instead for 
Did you mean: 

B-L072Z-LRWAN1 don't run with external power

mise
Associate II

Hi,

the program does not start if I connect a second usb power supply (or external power supply). The MCU runs normally when a st-link is connected. I tried a simple program - LED blink. The voltage on the MCU is good and the power LD6 is on. Any fuse or lock?

Thank you

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6

Make sure you have current ST-LINK firmware, and that NRST is not being held low.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mise
Associate II

ST link FW is new V2.33.25 now and NRST is high. It runs normally if both power are connected. The program will stop if I disconnect the st-link. The LED stays on (only stop - no reset).

What are you configuring as a clock source? 8MHz HSE?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mise
Associate II

I use internal HSI 16 MHz. The board has no soldered external crystal

The ST-LINK supplies an 8 MHz signal, the Murata has an 32 MHz TCXO

Run these things from batteries here. Check jumper settings.

Perhaps output diagnostics via a UART so you better understand what's happening internally.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mise
Associate II

ok, I'll try to find something

Thank you