cancel
Showing results for 
Search instead for 
Did you mean: 

About the radio frequency parameters and distance of WL33.

WWang.15
Associate II

Dear ST experts.

We are a module manufacturer. We have designed a module based on WL33. We have been using ST's dk board for verification. However, when we tested the distance, the original dk board was about 200 meters. With a 20dbm and -12X sensitivity, we have high expectations for this chip. Do you have ST distance test reports and parameters?
2. If our deviation is <2.5Khz, does it mean that we need to replace the TCXO?

 

B.R. Weili Wang.

12 REPLIES 12

Hello Weili,

I propose to evaluate the performances of two RF settings:

First RF configuration:

  • Data rate=200 kbps
  • Frequency deviation = 100 kHz
  • Channel filter= 400 KHz
  • DSSS = 16

Second RF configuration:

  • Data rate=100 kbps
  • Frequency deviation = 50 kHz
  • Channel filter= 200 KHz
  • DSSS = 16

Regards

Saverio


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Saverio.

Regarding the DSSS setting, is it the Spread Factor in the GUI?

WWang15_0-1737760067080.png

 

Saverio GRUTTA
ST Employee

Hello Weili,

Yes, It is the Spread Factor.  

Regards

Saverio


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.