cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-TOUCHGFX 4.15.0 is out

Martin KJELDSEN
Chief III

Hi Everyone,

If you haven't noticed by now, X-CUBE-TOUCHGFX 4.15.0 is out, available from CubeMX 6.0+ and from st.com as a zip (Also installable through CubeMX).

Main features:

  1. Designer: Built in support for Graph widget!
  2. Generator: Option to use Flash Reader (limited to 16-bit apps atm) to make direct use of a non-memory mapped flash with the LCD classes and avoid having to cache images.
  3. Improved performance of Partial Framebuffer Strategy for low-cost solutions (e.g. G0)

Here's the documentation for 4.15.0: https://support.touchgfx.com/

/Martin

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Bob Bailey
Senior

CubeIDE has an update also, curious what the details are there.

someone else posted a link to the changelog, it is here: https://support.touchgfx.com/docs/miscellaneous/changelog

the download page still says 4.15, but the file you get is 4.16 , in the designer, the tooltip for the Gauge widget is wrong.

Installed 4.16, everything seems like its working ok

It's just bad UI - When you're selecting a version you're actually selecting an OLD version. So the default is 4.16.0 unless you specifically choose a version - in this case you can only choose old ones.

/Martin