cancel
Showing results for 
Search instead for 
Did you mean: 

why the touch point and the displayed position are exactly opposite?

LLiao.1
Associate II

Hello, 

I used the SMT32F429i-DISC1 and TouchGFX follow the user guide

coding, why the touch point and the displayed position are exactly opposite?

For example, if my button is on the far left, I have to press the far right position of panel to respond?

Thanks

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
Martin KJELDSEN
Chief III

Which application template are you using from TouchGFX Designer?

Martin KJELDSEN
Chief III

I'll ask with the team responsible for ATs if they're aware of any current issues with the new 429-disc board.

OHenr.1
Associate II

Hello,

I got the blue board MB1075-F429I-E01

I used TouchGFXdesigner 4.14.0

I upgraded now to 4.16.1 , This version works now with my board, it has a different board selector and produces the right code.

The compiled binary firmware file from the board support page does not work with my board.

/Oliver

Thanks for the feedback, @OHenr.1​ 

MPasc.3
Associate

Hello guys,

Did you guys find a solution for this problem? I am using TouchGFX 4.18.1 and the displayed positions are still reversed.

Thank you!

AAdam.2
Associate II

Not sure if this helps anyone, but I had this issue when I choose the wrong stm32f429 variant.. D1 instead of E1.