cancel
Showing results for 
Search instead for 
Did you mean: 

Where do I put Texts::setLanguage(id) on start up of my system?

Loppi
Associate III

Hi everyone,

The text translation functionality of TouchGFX is awesome and implemented easily by just adding another language and implementing the code for the call of the setLanguage(id) function. I just wondered were I would put an initial call of this function after a system reboot. The currently selected language is saved in the flash section of the STM32 µcontroller and is being load to ram when the system starts.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0