2018-03-27 7:21 AM
Hi there folks!
I just wanted to know if it is possible to use the STM32F429I-DISC1 to test different external displays. The appropriate pins are provided via P1 and P2 but as far as I have understood the schematics the integrated display is allways connected with the MCU and there is no chance to disconnect that display or power it off.
I hope I am wrong
best regards
Benjamin
#stm32f429i-disc1 #external-display #lcdSolved! Go to Solution.
2018-03-28 1:02 AM
HI Benjamin,
the STM32F429i-disco is one of the most moddable disco boards available. To get some inspiration how to add another TFT to your STM32F429i-disco have a look at my webpage:
http://www.dasrotemopped.de/index.php?var=projekte&nr=21
Drive the LTDC in 16 bit mode and attach any direct driven TFT to the board. To save some power consumption, you can remove the onboard TFT (fastened with double sided duct tape) with a knive (be carful not to cut youself or damage the board). It is not neccesary to remove the onboard TFT if you use LTDC for your external TFT. Just disable the background LED and set your timings to the LTDC needed for your external TFT. Be aware that the power supply of the disco Board may be too weak to supply your external TFT and an external PSU is needed.
Have fun modding the STM32F429i-disco,
Markus.
2018-03-28 1:02 AM
HI Benjamin,
the STM32F429i-disco is one of the most moddable disco boards available. To get some inspiration how to add another TFT to your STM32F429i-disco have a look at my webpage:
http://www.dasrotemopped.de/index.php?var=projekte&nr=21
Drive the LTDC in 16 bit mode and attach any direct driven TFT to the board. To save some power consumption, you can remove the onboard TFT (fastened with double sided duct tape) with a knive (be carful not to cut youself or damage the board). It is not neccesary to remove the onboard TFT if you use LTDC for your external TFT. Just disable the background LED and set your timings to the LTDC needed for your external TFT. Be aware that the power supply of the disco Board may be too weak to supply your external TFT and an external PSU is needed.
Have fun modding the STM32F429i-disco,
Markus.
2018-03-28 4:13 AM
Hey Markus,
thx for your detailed answer. This sounds perfect and exactly for what I need.
best regards
Benjamin
2018-04-11 10:45 AM
A very important hint on using external displays:
It is NOT possible to use the discovery board to test 24Bit RGB LCDs because the appropriate pins are used for the 64Mbit external SRAM. Very sad.
2018-04-12 5:50 AM
Hi Benjamin,
if you need a Discovery Board with 24 bit TFT Support just try the STM32F746G-Disco :
http://www.dasrotemopped.de/index.php?var=projekte&nr=22
If you do the same trick as with the STM32F429i-disc1, removing the original onboard TFT, you get access to the 24 bit LTDC interface.
http://www.dasrotemopped.de/bilder/stm32f746g-disco_vga.jpg
More challenging to solder than the STM32F429i-disc1, but possible. Also inexpensive with some extra power of an STM32F7.
Happy modding,
Markus
2018-04-12 12:39 PM
Hey Markus,
thanks again for your fast and good answer. I wanted to use the appropriate processor for this project, because I will have a bigger test set up not only using a TFT. So a bigger processor will give me no benefit this time, as I will not have this computation power or available peripheral ressources. Maybe I will not have to use the internal LTDC. But this decision will be made next week
best regards
Benjamin