cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX v4.26.1 doesn't copy touchgfx_core.a to project folder?

daniel9
Associate

Is this version do not copy touchgfx_core.a to project folder? ex) Middlewares\ST\touchgfx\lib\core\cortex_m4f\IAR8.x

because I did generate code in touchGFX so automatelly remove the files in lib/core.

and i can't build on IAR because .ipcf file generated from touchGFX desinger need touchgfx_core.a of path above.

1 REPLY 1
JohanAstrup
ST Employee

Hello @daniel9.Which toolchain have you selected in STM32CubeMX?
Is the lib/core folder completely empty, or does it contain the library for a different compiler?

Can you share your project?

Best regards,
Johan