2021-06-08 4:05 PM
I'm using TouchGfx in Gray 4 mode. I have read the GFX documentation and I can't find the answer. I can't figure out how the data is stored in RAM. Consequently, I need to convert this Gray 4 to RGB565 to my FMC 16bit 8080 TFT-LCD. Any ideas how to do this? or additional references I should be reading? I'm using a 480 x 854 LCD.
Here is a failed attempt..
void TouchGFXHAL::copyFrameBufferBlockToLCD(const Rect rect)
{
__IO uint16_t* ptr;
int16_t row;
// For Gray4 only 4 bits per pixel
for (row = 0; row < (rect.width) ; row++)
{
ptr = getClientFrameBuffer() + rect.y + (row+ rect.x) * 120; // 480 x 854 LCD
LCD_IO_WriteMultipleDataGrey4((uint16_t*)ptr, 120);
}
}
void LCD_IO_WriteMultipleDataGrey4(uint16_t* pData, uint32_t Size)
{
uint32_t i;
for (i = 0; i < Size; i++)
{ // R 5bits G 6bits B 5 bits
FMC_BANK1_WriteData( ((pData[i]&0xF000)<<0) | ((pData[i]&0xF000)>>5) | ((pData[i]&0xF000)>>12) );
FMC_BANK1_WriteData( ((pData[i]&0x0F00)<<4) | ((pData[i]&0x0F00)>>0) | ((pData[i]&0x0F00)>>8) );
FMC_BANK1_WriteData( ((pData[i]&0x00F0)<<8) | ((pData[i]&0x00F0)<<5) | ((pData[i]&0x00F0)>>4) );
FMC_BANK1_WriteData( ((pData[i]&0x000F)<<12) | ((pData[i]&0x000F)<<10) | ((pData[i]&0x000F)>>0) );
}
}
2021-06-08 10:24 PM
Your shifting nums >> << isnt right, check :beaming_face_with_smiling_eyes:
2021-06-09 12:25 PM
for (i = 0; i < Size; i++)
{ // R 5bits G 6bits B 5 bits
FMC_BANK1_WriteData( ((pData[i]&0xF000)<<0) | ((pData[i]&0xF000)>>5) | ((pData[i]&0xF000)>>11) );
FMC_BANK1_WriteData( ((pData[i]&0x0F00)<<4) | ((pData[i]&0x0F00)>>1) | ((pData[i]&0x0F00)>>7) );
FMC_BANK1_WriteData( ((pData[i]&0x00F0)<<8) | ((pData[i]&0x00F0)<<3) | ((pData[i]&0x00F0)>>3) );
FMC_BANK1_WriteData( ((pData[i]&0x000F)<<12) | ((pData[i]&0x000F)<<7) | ((pData[i]&0x000F)<<1) );
}ok this is correct now, right?
Thanks, Kevin
2021-06-09 10:02 PM
Seems right now, and too exist second choice use DMA2D L4 CLUT conversion for offload MCU. This enable choice some colors not only gray...