cancel
Showing results for 
Search instead for 
Did you mean: 

Touchgfx display is not displaying anything

ITena.1
Associate II

Hello,

I am working on a project with stm32f769i-eval and touch gfx designer(4.13.0) .

I select my board as application template then I try both using a blank template or any of the examples that are provided.

After generating the code, I try to run the project on my target and even though it doesn't fail my screen is not displaying anything. (If I run on the simulator it works perfectly).

What should I do?

Thx,

Irene

This discussion is locked. Please start a new topic to ask your question.
25 REPLIES 25
TJoha.1
Associate II

The workaround is working for me. Thank you very much.

Good luck further investigating!

Regards,

Tim

thanks ;) Good luck with your project

Hi @Romain DIELEMAN​ ,

I had the same problem, and your workaround worked for me. But isn't there a formal fix yet? I'm using TouchGFX Designer 4.16.1.

Thanks

Hi,

There should be a fix soon. It will most likely be a new application template with the revision specified.

/Romain

Actually it will not be a new TouchGFX Board Setup (new name for "Application Template") but just a new version of the existing one for the STM32F769-eval. It should be up next week or the week after.

/Romain

MGünt.1
Associate

*edited*