cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX Custom Application FLASH Overflow Issue & QSPI Memory Setup

naveen
Associate III

 

 

Subject: TouchGFX Custom Application FLASH Overflow Issue & QSPI Memory Setup

Greetings Team,

I’m new to STM32 TouchGFX and trying to create a custom TouchGFX application following How to integrate TouchGFX in a custom board (The long way round) - YouTube

After setting everything up, I encountered the following error during the build:

`.text' will not fit in region `FLASH' region `FLASH' overflowed by 296512 bytes 

 

I understand that my MCU has only 128KB of Flash, which is insufficient for TouchGFX. I want to configure TouchGFX to use only SDRAM instead of Flash. How does TouchGFX utilize SDRAM, and how can I correctly set it up for this purpose?

Additionally, when comparing my custom application to the STM32H7 Dev Board example, I noticed different memory configurations in the Cortex-M7 section under System Core. Specifically, I don’t fully understand how QSPI Flash is mapped as two memory regions starting from 0x90000000.

I've attached a screenshot for reference. Kindly guide me on resolving the FLASH overflow issue and understanding the QSPI memory setup.

Thanks in advance!

Screenshot 2025-02-13 164135.png

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Hello @Osman SOYKURT 

Thank you for your reply.

Indeed, the linked script is something I am still not sure how exactly it works.

Anyway, what I have done is to use the "TBS"  in the Designer and open it in the CubeIDE, where the LTDC was updated for the custom LCD.  Indeed, the GPIOs are the same as for the original LCD that comes with the STM32H750B-DK. For example, I can use and preview the primitive graphics, like circles, etc. via the original LTDC util functions in Keil just fine. However, I do not have much luck with setting up the TouchGFX in CubeIDE. 

Anyway, I have managed the compilation, and I get "some graphics" on my display.

Creating a new forum post.

Best.

/*
******************************************************************************
**
**  File        : LinkerScript.ld
**
**  Author		: Auto-generated by STM32CubeIDE
**
**  Abstract    : Linker script for STM32H750XBHx Device from STM32H7 series
**                      128Kbytes FLASH
**                      128Kbytes DTCMRAM
**                      64Kbytes ITCMRAM
**                      512Kbytes RAM_D1
**                      288Kbytes RAM_D2
**                      64Kbytes RAM_D3
**
**                Set heap size, stack size and stack location according
**                to application requirements.
**
**                Set memory bank area and size if external memory is used.
**
**  Target      : STMicroelectronics STM32
**
**  Distribution: The file is distributed as is without any warranty
**                of any kind.
**
*****************************************************************************
** @attention
**
** <h2><center>&copy; COPYRIGHT(c) 2020 STMicroelectronics</center></h2>
**
** Redistribution and use in source and binary forms, with or without modification,
** are permitted provided that the following conditions are met:
**   1. Redistributions of source code must retain the above copyright notice,
**      this list of conditions and the following disclaimer.
**   2. Redistributions in binary form must reproduce the above copyright notice,
**      this list of conditions and the following disclaimer in the documentation
**      and/or other materials provided with the distribution.
**   3. Neither the name of STMicroelectronics nor the names of its contributors
**      may be used to endorse or promote products derived from this software
**      without specific prior written permission.
**
** THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
** AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
** IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
** DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
** FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
** DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
** SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
** CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
** OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
** OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
**
*****************************************************************************
*/

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1);	/* end of "RAM_D1" Ram type memory */

_Min_Heap_Size = 0x1000;	/* required amount of heap  */
_Min_Stack_Size = 0x1000;	/* required amount of stack */

/* Memories definition */
MEMORY
{
  DTCMRAM      (xrw)    : ORIGIN = 0x20000000,   LENGTH = 128K
  ITCMRAM      (xrw)    : ORIGIN = 0x00000000,   LENGTH = 64K
  RAM_D1       (xrw)    : ORIGIN = 0x24000000,   LENGTH = 512K
  RAM_D2       (xrw)    : ORIGIN = 0x30000000,   LENGTH = 288K
  RAM_D3       (xrw)    : ORIGIN = 0x38000000,   LENGTH = 64K
  SDRAM        (xrw)    : ORIGIN = 0xD0000000,   LENGTH = 8M
  FLASH	       (xrw)    : ORIGIN = 0x90000000,   LENGTH = 2048K
  ASSETS_FLASH (r)      : ORIGIN = 0x90200000,   LENGTH = 126M
  BOOTLOADER   (xrw)    : ORIGIN = 0x08000000,   LENGTH = 128k
}

TARGET(binary) /* specify the file format of binary file */
INPUT (../../ExtMem_Boot/bootloader.bin) /* bootloader bin file path (relative to the output folder)*/
OUTPUT_FORMAT(default) /* restore the out file format */

/* Sections */
SECTIONS
{
  .bootloader :
  {
    . = ALIGN(4);
    KEEP(../../ExtMem_Boot/bootloader.bin)
  } > BOOTLOADER

  /* The startup code into "FLASH" Rom type memory */
  .isr_vector :
  {
    __ICFEDIT_intvec_start__ = .;
    . = ALIGN(4);
    KEEP(*(.isr_vector)) /* Startup code */
    . = ALIGN(4);
  } >FLASH

  /* The program code and other data into "FLASH" Rom type memory */
  .text :
  {
    . = ALIGN(4);
    *(.text)           /* .text sections (code) */
    *(.text*)          /* .text* sections (code) */
    *(.glue_7)         /* glue arm to thumb code */
    *(.glue_7t)        /* glue thumb to arm code */
    *(.eh_frame)

    KEEP (*(.init))
    KEEP (*(.fini))

    . = ALIGN(4);
    _etext = .;        /* define a global symbols at end of code */
  } >FLASH

  /* Constant data into "FLASH" Rom type memory */
  .rodata :
  {
    . = ALIGN(4);
    *(.rodata)         /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)        /* .rodata* sections (constants, strings, etc.) */
    . = ALIGN(4);
  } >FLASH

  .ARM.extab (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */ 
  {
    . = ALIGN(4);
    *(.ARM.extab* .gnu.linkonce.armextab.*)
    . = ALIGN(4);
  } >FLASH

  .ARM (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */ 
  {
    . = ALIGN(4);
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
    . = ALIGN(4);
  } >FLASH

  .preinit_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__preinit_array_start = .);
    KEEP (*(.preinit_array*))
    PROVIDE_HIDDEN (__preinit_array_end = .);
    . = ALIGN(4);
  } >FLASH

  .init_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array*))
    PROVIDE_HIDDEN (__init_array_end = .);
    . = ALIGN(4);
  } >FLASH

  .fini_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
  {
    . = ALIGN(4);
    PROVIDE_HIDDEN (__fini_array_start = .);
    KEEP (*(SORT(.fini_array.*)))
    KEEP (*(.fini_array*))
    PROVIDE_HIDDEN (__fini_array_end = .);
    . = ALIGN(4);
  } >FLASH

  /* Used by the startup to initialize data */
  _sidata = LOADADDR(.data);

  /* Initialized data sections into "RAM_D1" Ram type memory */
  .data :
  {
    . = ALIGN(4);
    _sdata = .;        /* create a global symbol at data start */
    *(.data)           /* .data sections */
    *(.data*)          /* .data* sections */

    . = ALIGN(4);
    _edata = .;        /* define a global symbol at data end */

  } >RAM_D1 AT> FLASH

  /* Uninitialized data section into "RAM_D1" Ram type memory */
  . = ALIGN(4);
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section */
    _sbss = .;         /* define a global symbol at bss start */
    __bss_start__ = _sbss;
    *(.bss)
    *(.bss*)
    *(COMMON)

    . = ALIGN(4);
    _ebss = .;         /* define a global symbol at bss end */
    __bss_end__ = _ebss;
  } >RAM_D1

  /* User_heap_stack section, used to check that there is enough "RAM_D1" Ram  type memory left */
  ._user_heap_stack :
  {
    . = ALIGN(8);
    PROVIDE ( end = . );
    PROVIDE ( _end = . );
    . = . + _Min_Heap_Size;
    . = . + _Min_Stack_Size;
    . = ALIGN(8);
  } >RAM_D1

  /* Remove information from the compiler libraries */
  /DISCARD/ :
  {
    libc.a ( * )
    libm.a ( * )
    libgcc.a ( * )
  }

  .ARM.attributes 0 : { *(.ARM.attributes) }



  FontFlashSection :
  {
    *(FontFlashSection FontFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >ASSETS_FLASH

  TextFlashSection :
  {
    *(TextFlashSection TextFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >ASSETS_FLASH

  ExtFlashSection :
  {
    *(ExtFlashSection ExtFlashSection.*)
    *(.gnu.linkonce.r.*)
    . = ALIGN(0x4);
  } >ASSETS_FLASH

  BmpCacheSection (NOLOAD) : { *(BmpCacheSection) } >SDRAM
  TouchGFX_Framebuffer (NOLOAD) : { *(TouchGFX_Framebuffer) } >SDRAM
  TouchGFX_Framebuffer1 (NOLOAD) : { *(TouchGFX_Framebuffer1) } >SDRAM
  TouchGFX_Framebuffer2 (NOLOAD) : { *(TouchGFX_Framebuffer2) } >SDRAM
  Video_RGB_Buffer (NOLOAD) : { *(Video_RGB_Buffer) } >SDRAM

}