TGFX 4.18: RAM problem with the new video widget
Dear all,
I have a problem with the new video widget in combination with the STM32F769NI-DISCO (MIPI DSI display 800x480 px, JPEG HW en-/decoder, 16 MB ext RAM, 64 MB ext QSPI Flash).
If I create with the TGFX designer 4.18 a new video example project with this board, the video runs without problems. If I change the video to the 800x480 sample video and increase also the video frame buffer in CubeMx it's not possible to build the project because the RAM size is out of limit.
It seems, that TGFX use just the internal RAM for the video framebuffer.
So the question is:
Is it possible to switch the video framebuffer also to the external RAM?
And if yes, how can I do this?
Thank you in advance.
BR,
John