2018-04-25 11:33 PM
Hi friends,
I would like to learn the programming of the TFT LCD module (p/n: MB895/S, SPI interface) which comes with the the evaluation board STM32 L073Z-Eval. However, I just can't even find the programming specifications of this LCD module or information about the LCD driver IC (SPI?) for this module.
Could anyone help me on this?
Thank you very much!
Hua
#tft-lcd-mb895/s-programming2018-04-27 12:57 AM
I made some progresses and managed to get the TFT LCD initialization done, as well as simple display using the STM32 driver provided under the BSP.