2025-03-17 1:17 AM
Hello
So, I want to generate a test application, but I cannot load these on my board. Does that problem is normally because we never can upload a test application or what is the Problem here, I also added some parts to the Test application, but I can still not load up. I think I am a little bit stuck right now. Maybe one can help me. Thanks!
( I am useing the TouchGFX Designer 4.24.0)
Solved! Go to Solution.
2025-03-17 2:56 AM
When you create your project, did you chose the right board ? If you chose simulator it will not work.
2025-03-17 2:43 AM
Hello @Bea_12,
What board did you chose when you create the application ?
Br,
2025-03-17 2:52 AM
Oh sorry I forgot, I am using the STM32F746G -Discovery Board right now.
2025-03-17 2:56 AM
When you create your project, did you chose the right board ? If you chose simulator it will not work.
2025-03-17 3:09 AM
Oh wow, you were absolutely right! I thought I had chosen the correct board, but I didn’t. Thanks so much! Now, I really hope it works.
2025-03-17 3:58 AM
You are welcomed, if your issue is solved, please mark the best answer so other members can easily find the solution.