2024-02-27 07:04 PM
Hello. Recently I received an STM32U5G9J-DK2 board which I purchased earlier this year. I want to ask for the Out-of-Box Demo of this board for backup since I find it really stunning and I want some reference for my own TouchGFX GUI application design. So, where should I go for asking? Or is this demo available in source project or binary file or neither makes sense? Can I, as a student, be able to get a binary file version of it?
Looking forward to your replies. Thanks in advance.
Solved! Go to Solution.
2024-03-14 08:05 AM
Yes, the demos are a bit different. We cannot share that project with you, but I can send you the binary file
Good luck
2024-02-28 06:10 AM
Hello @Nathan_Xi ,
The OBD for STM32U5G9J-DK2 is based on the TouchGFX Demo 7 that is available on TouchGFX Designer. And, you can access the source code as well.
I hope this answers your question.
2024-03-07 03:55 AM
Err...thank you but I suppose that it's not the same demo software however, the original one has a vector map subdemo and a animated vector font subdemo. That's apparently not the same. Is there an original version of that?
2024-03-14 08:05 AM
2024-03-28 12:44 AM
Thank you so much!I always expected that a binary file could be given. This really proves to be a good "solution" to this blog.
2024-04-02 12:16 AM
You're very welcome!