cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L476 with custom segment LCD aka LCD glass aka Passive LCD

Silas Valera
Senior
Posted on July 02, 2017 at 23:38

Hello,

I have an application where I need the following:

1. Lowest possible power conusmption - in any mode run/standby/sleep - it is a battery powered application

2. The controller also includes segment LCD driver - driving up to min 64 segments

3. The controller also keeps the segment LCD live (no turning off the LCD) in sleep/standby mode 

Refering to the reference manual / data sheet for STM32L476, I found that this is a suitable controller I can use for my application.:

Q1. Has anyone any experience using STM32L4 in application for driving segment LCD? Can anyone please help me with any example / document?  

Q2. Further for the segment LCD, how does the common and segment pins layout work?

Any primer or document will be really helpful and very much appreciated..

Thanks in advance!

best

Silas  

#segment-lcd
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

Hello @Jde J.1253​ 

You should download the latest version of STM32CubeL4 V1.15.0 from st.com

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Please start a new thread stating your problem, don't extend on years old threads (if you need, link to them).

You can preview the Cube stuff also at github, e.g. https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Projects/STM32L476G-EVAL/Examples/LCD/LCD_SegmentsDrive , but it will probably require files from other directories of the "library", too.

I have a simplistic clock project using the LCD glass on the 'L4 DISCO at www.efton.sk/STM32 , that might be a starting point, too, if you prefer register-level approach to "libraries".

JW