Skip to main content
tengaimakyou
Associate II
June 24, 2012
Question

STM32L-discovery with IAR EWARM : Weird LCD display

  • June 24, 2012
  • 5 replies
  • 1669 views
Posted on June 24, 2012 at 23:13

Hello

I recently bought a STM32L-discovery and i try to print some message on the lcd display using some examples coming with IAR EWARM

(LCD_SegmentsDrive for example).

But when i use the function LCD_GLASS_DisplayString(''TEST''), the lcd hilights some segments in incomprehensible order.

i first tried to execute the program in RAM using ''Download and debug'' without achieving to print some readable message.

and when i pushed on reset, i had the normal message of the default program so i suppose than the board is OK.

I then tried Flashing memory using ''download active application'' but without success.

the Projet->option->debugger driver is set on ST-LINK and ST-LINK Reset on Normal, CLock Set up on 32.0 Mhz.

I let the jumpers on their default positions (2 jumpers on ST-Link and the jumper on JP1 on)

i am new to both EWARM and STM32 so if someone can help me.

Thanks.

#linker-bin-stm32-ewarm #stm32-discovery-iar-ewarm-lcd
This topic has been closed for replies.

5 replies

tengaimakyou
Associate II
June 26, 2012
Posted on June 26, 2012 at 13:52

I change some parameters using this document :

http://netstorage.iar.com/SuppDB/Public/SUPPORT/004364/Programming%20BIN%20by%20EWARM%20_ST_.pdf

but i now have a build problem :

    Fatal Error[Li001]: could not open file ''C:\Program Files\IAR Systems\Embedded Workbench 6.4 Evaluation\arm\examples\ST\STM32L1xx\STM32L1xxHD_StdPeriph_Lib\Project\STM32L1xx_StdPeriph_Examples\LCD\ LCD_SegmentsDrive\demo.bin''

    Error while running Linker

 I don't know if it means that  demo.bin is not found (i though that it was the purpose of the build to create it) or can't be accessed.

When i create an empty demo.bin file, it builds but the file is not modified.

I am not sure to correctly configure Linker->Input, and the main difference with the document i found is that i use libraries.

I though that all this settings were made in by the example project. I use STM32L1xxHD_StdPeriph_Lib\ because i have read that the STM32L152RBT6 of the STM32L-discovery was a High density MCU and in Options -> device i put ST STM32L152xB.

If somebody have any suggestions.

Thanks

Tesla DeLorean
Guru
June 26, 2012
Posted on June 27, 2012 at 00:46

If you have the .bin or .map files open in other applications this will cause issues.

Windows 7 does not like User files under ''\Program Files'' it's generally considered bad form.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ss882
Associate II
August 16, 2012
Posted on August 16, 2012 at 20:18

Hey Pansoul,

I am also sailing in the same boat now...!

Did you solve that problem?

Can you help me??

Thanks,

Shweta

Tesla DeLorean
Guru
August 16, 2012
Posted on August 16, 2012 at 21:57

Try putting your projects in

C:\Users\WHOMEVER\IARProjects\

Or some other directory where you can actually have full access rights to your files, and AV software won't throw fits.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
tengaimakyou
Associate II
September 27, 2012
Posted on September 27, 2012 at 15:46

Hello

Sorry for the late response. I don't know if you finally come up with EWARM and clive1 solution. As for me, i moved to Keil µVision and it works.