cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H board with LCD screen and MCU DAC outputs

FEory.1
Associate

Hello,

I am new to the discovery line up.

I am looking for a ST32H board with fast direct MCU connection LCD similar to the STM32H745-DISCO with 2 MCU DAC outputs. I can't use the codec DAC because the latency is too long. I see only one DAC connected to a pin on the STM32H745-DISCO. Suggestions for a board?

Is there a real fast way for me to check for DAC pins on the MCU and see if they are routed? I am currently just checking pinouts sample projects with cubeMX of various boards and comparing with schematics.

Thanks,

Frank

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0