Skip to main content
nsabo.1
Associate III
November 9, 2022
Question

stm32f429 2 ltdc layer addreesed in Sdram

Hi, I initialized 2 layers in LTDC to show 2 images, which was done directly by addressing them from flash.

That was fine till I want to set 2 layers in my SDRAM.

application note has said the first one should be addressed in 0xc0000000 and the second one should be configured in a bank addition to first layer.

The problem is 2 layers independently work but to enable them at the same time, they won't work properly.

Have some one faced with this problem?

what should I do to enable them at the same time?

stm 32f429

LTDC is configured in 16 bits.

This topic has been closed for replies.

2 replies

MM..1
Super User
November 9, 2022

Why you need two layers in ram?

Is layers too RGB565 ?

How dotclock you use for LTDC? ...

show layer2 addr too. for check.

What is wont work prop...

nsabo.1
nsabo.1Author
Associate III
November 21, 2022

Hi, sorry for my late reply, I didn't understand what dotclock in LTDC is.

I finally set 2 layers in SDRAM but, I got some tempering with images I thought that was due to my SDRAM configuration.

I meant it is possible to address directly your buffers which can be images... in SDRAM, but you should know to address them n 2 different SDRAM banks.

Now, I have another question:

I am using TOUCHGFX, in my project I have to display 12 graphs in two columns (2*6), I want to have grids behind my graphs for this case I don't use minor and major grid lines for graphs, I wrote them manually by lines....

when I use vertical frontline for my dynamic graph, the line erase my behind grids too.

Is there any idea to help me frontline doesn't erase the behind grids?