2017-10-25 5:51 AM
Hello All,
I am first time working on DCMI with STM32f4 series micro controller.
We are planing to interface DCMI camera with STM32f407 Micro controller.
Camera Resolution is '2592x1944' and Image size goes up to 512kb ~ 2MB.
Camera module consist of ov5642 CMOS.
We have already interfaced Memory card for storage of data.
Is there any external memory(Buffer) is required while camera image capturing is in process?
Is there any possibility to store image directly in to Memory card over SPI interface?
#dma #memory #stm32f407 #dcmi #ov56422017-10-25 8:41 AM
You'd need to store the image somewhere if you can't process it on-the-fly, SPI to SD Card is going to have woeful performance, SDIO would be significantly better, but even back-of-the-envelope math suggests you aren't going to be able to stuff 14-bit @ 54 MHz onto 4-bit @ 24 MHz, let alone onto a 1-bit interface.
Perhaps look at a FIFO if external memory is undesirable, say AL422B or AL462 for 2K type imagery
http://www.averlogic.com/AL422B.asp
2017-10-25 10:07 PM
Hello Sir,
Thanks for your reply.
I want to use STM32f407 Controller so can you suggest us any kind of FiFo or RAM which is suitable with STM32f407 ?
I am newbie RAM interfacing with STM32f407 micro controller. Can you Provide us good reference on RAM interface with STM32f407 Controller ?
Below are the Camera Pin Specification.
Pin No.
PIN NAME
TYPE
DESCRIPTION
1
VCC
POWER
3.3v Power supply
2
GND
Ground
Power ground
3
SCL
Input
Two-Wire Serial Interface Clock
4
S
DATA
Bi-directional
Two-Wire Serial Interface Data I/O
5
VSYNC
Output
Active High: Frame Valid; indicates active frame
6
HREF
Output
Active High: Line/Data Valid; indicates active pixels
7
PCLK
Output
Pixel Clock output from sensor
8
XCLK
Input
Master Clock into Sensor
9
D
OUT
9
Output
Pixel Data Output 9 (MSB)
10
D
OUT
8
Output
Pixel Data Output 8
11
D
OUT
7
Output
Pixel Data Output 7
12
D
OUT
6
Output
Pixel Data Output 6
13
D
OUT
5
Output
Pixel Data Output 5
14
D
OUT
4
Output
Pixel Data Output 4
15
D
OUT
3
Output
Pixel Data Output 3
16
D
OUT
2
Output
Pixel Data Output 2 (LSB)
17
PWDN
Input
Power down
18
RSV
NC
Reserved
19
D
OUT
1
Output
Pixel Data Output 1(10bit mode)
20
D
OUT
0
Output
Pixel Data Output 0 (10bit mode)