cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 and 1024x600 display refresh problem

nicola2
Associate II
Posted on June 30, 2015 at 16:02

Hello,

I'm using stemwin 5.26 on STM32F429IIT6 using LCD controller and freertos. my display is 1024 x 600. I started to implement some simple windows, but I see that refresh of the window causes a visible frame corruption. I made and attached a small video to explain clearly the issue.

I saw that using only on later (GUI_NUM_LAYERS 1) seems to cancel the issue. I cannot focus if the problem is in the ltdc configuration, dma2d config or STemWin libs.

Here code snippets of what I have in the program.

main()

{  

  /*** [.....] ****/

  /* Initialize GUI */

  GUI_Init();

  

  osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);

  defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);

  

  osThreadDef(GUI_Thread, GUIThread, osPriorityLow, 0, 20 * configMINIMAL_STACK_SIZE);

  osThreadCreate(osThread(GUI_Thread), NULL); 

  

  /* Start scheduler */

  osKernelStart();

/**************************************************************************************/

  static void GUIThread(void const * argument)

    { 

    GUI_SelectLayer(1);    

    GUI_SetColor (GUI_YELLOW);

    GUI_FillRect(600,300,1024,600);

    GUI_SetColor (GUI_BLUE);

    GUI_FillRect(20,10,500,500);

    

    k_InitMenu(); 

    

    while(1) 

        {

        LED_Toggle(LED1);

        LED_Toggle(LED2);

        GUI_Delay(100);

        }

    }

    

/**************************************************************************************/

void k_InitMenu(void) 

{

  WM_SetCallback(WM_HBKWIN, _cbBk);

  

  GUI_SelectLayer(1);

  WM_CreateWindowAsChild(0, 0, 1000, 25, WM_HBKWIN, WM_CF_SHOW | WM_CF_HASTRANS | WM_CF_MEMDEV, _cbStatus, 0);

}

    

/*******************************************************************************

  * @brief  Callback routine of desktop window status.

  * @param  pMsg: pointer to data structure of type WM_MESSAGE

  * @retval None

  */

static void _cbStatus(WM_MESSAGE * pMsg) 

    {

    int xSize, ySize;

    static uint8_t TempStr[50];

    static WM_HTIMER hTimerTime;

    static uint8_t tmp;

    static uint8_t bmp_res2;

    RTC_TimeTypeDef   RTC_Time;

    RTC_DateTypeDef   RTC_DateStructure;

    uint8_t sec, min, hour, day, month;

    uint16_t year;

    WM_HWIN hWin;

    hWin = pMsg->hWin;

    switch (pMsg->MsgId) 

        {

        case WM_CREATE:

        hTimerTime = WM_CreateTimer(hWin, ID_TIMER_TIME, 1000, 0);

        break;

        case WM_DELETE:

        WM_DeleteTimer(hTimerTime);

        break;

        case WM_TIMER:

        if( WM_GetTimerId(pMsg->Data.v) == ID_TIMER_TIME)

            {

            WM_InvalidateWindow(pMsg->hWin);

            WM_RestartTimer(pMsg->Data.v, 1000);

            }

        break;

        case WM_PAINT:

        xSize = WM_GetWindowSizeX(hWin);

        ySize = WM_GetWindowSizeY(hWin);

        /* Draw background */

        GUI_Clear();

        

        GUI_SetColor(0x008d00);

        GUI_FillRect(0, 0, xSize , ySize - 3);

        GUI_SetColor(0x808080);

        GUI_DrawHLine(ySize - 2, 0, xSize );

        GUI_SetColor(0x404040);

        GUI_DrawHLine(ySize - 1, 0, xSize );

        /* Draw time & Date */

        GUI_SetTextMode(GUI_TM_TRANS);

        GUI_SetColor(GUI_WHITE);

        GUI_SetFont(GUI_FONT_13B_ASCII);

        k_GetTime(&RTC_Time);

        sec    =  RTC_Time.Seconds;

        min    =  RTC_Time.Minutes;

        hour   =  RTC_Time.Hours;

        k_GetDate(&RTC_DateStructure);

        sprintf((char *)TempStr, ''%02d:%02d:%02d'', hour , min, sec);

        GUI_DispStringAt((char *)TempStr, xSize - 70, 4);

        year =  RTC_DateStructure.Year + 2014;

        month =  RTC_DateStructure.Month;

        day =  RTC_DateStructure.Date;

        if((day > 0) && (day <= 31) && (month > 0)&& (month <= 12) && (year >= 1900))

            {sprintf((char *)TempStr, ''%02d, %s, %04d'', day , strMonth[month-1], year);}

        else

            {sprintf((char *)TempStr, ''01, January, 2014'');}

        GUI_DispStringHCenterAt((char *)TempStr, xSize / 2, 4);

        GUI_DispStringAt( (char *)TempStr, 50, 4);

        break;

        default:

        WM_DefaultProc(pMsg);

        break;

        }

    }

#display-stm32f4-lcd
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
nicola2
Associate II
Posted on July 07, 2015 at 11:15

After few attempts, I found that reducing the speed of LTDC peripheral can cancel the problem.

My 1024x600 display can support higher clock and the LVDS converted the same. I have to decrease to 20 MHz instead of 32 MHz. Is there some limits I have to consider?

Best Regards