cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube_FW_L4_V1.14.0, cannot find TouchGFX source code of 32L4R9IDISCOVERY ! Where can I get it ?

Acai.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Martin KJELDSEN
Chief III

Please be more specific. Are you talking about a specific demo or example in the Cube FW packs?

/Martin

Acai.1
Associate II

Hi Martin,

Acai.1
Associate II

STM32Cube_FW_L4_V1.14.0\Projects\32L4R9IDISCOVERY\Demonstrations\TouchGFX without source code.

Acai.1
Associate II

if using TouchGFX 4.12.3 Designer to generate the "TouchGFX Watch" project for 32L4R9IDISCOVERY, it has IAR and gcc only, is there any Keil project ?

Acai.1
Associate II

More, any Good TouchGFX tutorial for helping us to change the LCD of 32L4R9IDISCOVERY to customer's one ?

Acai.1
Associate II

"TouchGFX Watch" can be run up on EVB 32L4R9IDISCOVERY, thank you.

Acai.1
Associate II

Here comes next question, how to modify it to use customer's 454x454 MIPI LCD ? any application note ? thank you !

No Keil project, but you could probably make it yourself.

I'll check if this is something i can share.