2023-09-15 3:31 AM
I'm using touchgfx 4.22 on a stm32h755zi mcu. The touchgfx run on the M7 core. The mcu is running at 480MHz.
The board is an internal board with a 800x480 display connected in parallel to the LTDC interface with a 18bit bus as shown below:
I use an rgb565 buffer in an external psram. Touchgfx settings are as follow:
And here the dma2d settings:
I've made a simple screen where there is a fade of a box of 800x480 pixel (all the screen) from gray color to transparent but this fade is very slow. With or without DMA, the result is the same.
Here a video of the fade: https://www.youtube.com/watch?v=OfER5-DQu4M
sorry for the poor video quality; however the screen starts in grey color and after 1 second the box in grey color disappears and another screen is shown. All of this with a fade effect.
And here it is how I made the fade; it's a simple interaction:
As far as I understand the fade duration should be 1s but it is 7-8 seconds. A part the wrong duration, the fade is quite sloppy with or without dma.
What am I doing wrong?
2023-09-18 7:17 AM
Any advice? I still don't understand why my graphic is not accelerated...
Or, do you think that this is the best performance I can achieve with this mcu?
2023-09-18 8:13 AM
Seems you use no OS implementation. Here is your job manage timing and seems not good.
2023-09-19 12:45 AM
I've choosen LTDC as Application Tick source as described here: https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-ltdc-parallel-rgb
and as you can see also in a screenshot in my first post; I mean this:
At the end of the documentation, I read this:
and looking through the code I see that the isVsyncAvailable() is called everytime LTDC generates an interrupt. The interrupt handler that manages this is: HAL_LTDC_IRQHandler.
So I think it is all managed correctly but I see it is all slow.
Or maybe I've to do some timing management but I don't know how. Do you have any link in the documentation that I can follow?
Thank you
2023-09-19 5:19 AM
LTDC clock in clock config ? In theory you require around 25MHz
Maybe your PLL dont work ok.
2023-09-19 6:16 AM
Yes it is set at 23MHz at the moment. I measured the dot clock on my tft with an oscilloscope and it is seems perfect and at 23MHz
2023-09-19 10:15 AM
? an external psram you mean OCTOSPI
Try read about LTDC optimise LCD-TFT display controller (LTDC) on STM32 MCUs - Application note
2023-09-20 1:46 AM
No I don't mean an OCTOSPI but a PSRAM
To be honest, I don't use a PSRAM since it's very difficult to find. However I am using a normal SRAM (a IS61WV102416FBLL-10TLI ) with 2 SN74LVC573APW latches and inverter for nadv.
The FMC clock is configured this way:
With some simple read/write test I've found the fastest clock we can achieve in order to have best performance. As far as I can understand the ram clock is enough to cover my display but I can be wrong. I don't find in the document you linked me, a section regards psram (only sdram, octospi, qspi flash) so I hope to have made my calculation well.
If I lower the FMC clock I see that the screen is corrupt so I think with this configuration the sram is fast enough.
What I don't understand is why if I set a 1s transition with fade, the whole cicle is 7-8seconds.
P.S.
I've tried also what it is described here: https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-measure-performance#performance-metrics
and measured with an oscilloscope the timings. The vsync signal seems to be generated every 17ms which seems correct to me.
2023-09-20 6:39 AM - edited 2023-09-20 6:46 AM
As explained in pdf. Displays can have many bottlenecks and one worse wins. For redraw in animation full screen 800x480x2 fade full is read recals write = around 138MB/s troughput over memory bus. Your memory is 3/1/1 clk 16bit wide then real speed is 229/2 little around required. Then next issues must exist , what holds bus ocupied...
Result is LTDC read framebuffer and send ok speed, but data in buffer is changed slow = animation skip frames.
Too double buffering make thiks worse... Try Performance | TouchGFX Documentation detect lost frames
2023-09-26 6:37 AM
Sorry for the delay here... I'm coming to the conclusion that accessing this external ram is slow but I don't know why or what I've to do for making it faster.
I've made some very simple benchmark in order to see how fast is writing/reading/modifying the whole psram area
uint16_t psramRead = 0 ;
int begin;
int end;
int TimeRead;
int TimeWrite;
int TimeModify;
uint16_t *psram = 0x60000000;
begin = HAL_GetTick();
for (uint32_t i=0; i<1048576; i++){
psram[i] = 0x0;
}
TimeWrite = HAL_GetTick() - begin;
begin = HAL_GetTick();
for (uint32_t i=0; i<1048576; i++){
psramRead = psram[i];
}
TimeRead = HAL_GetTick() - begin;
begin = HAL_GetTick();
for (uint32_t i=0; i<1048576; i++){
psram[i] += 2 ;
}
TimeModify = HAL_GetTick() - begin;In this test I see that
TimeWrite is around 170ms
TimeWrite is around 100ms
TimeWrite is around 180ms
This seems an enormous time for me. What am I doing wrong? Is there a way to make the access to the external ram faster?