Skip to main content
JNova.0
Associate III
February 2, 2024
Question

Slider with inverted MIN, MAX values

  • February 2, 2024
  • 0 replies
  • 846 views

Hello,
I'm working with a slider and ran into this problem.
When I define

setValueRange(0, 255);

and then I set the value

setValue(25);

so everything works. But I would like to turn the values on the slider. That means I will enter

setValueRange(255, 0);

At this moment, the restrictive conditions are poorly applied.

In the code for the slider I found the problem here:

int16_t Slider::valueToPosition(int value) const
{
 value = MIN(valueRangeMax, value);
 value = MAX(value, valueRangeMin);
...

In order for the slider to work for the range "0, 255" as well as for "255, 0", this code needs to be modified.
I used the following code. The original is in the comment and there is also code using if. Uncommented, the functional code is using a conditional expression, which may not be as readable:

int16_t Slider::valueToPosition(int value) const {
/*
// original
// value = MIN(valueRangeMax, value);
// value = MAX(value, valueRangeMin);
 
	if (valueRangeMax > valueRangeMin) {
		value = MIN(valueRangeMax, value);
		value = MAX(value, valueRangeMin);
	} else {
		value = MIN(valueRangeMin, value);
		value = MAX(value, valueRangeMax);
	}
*/
	value = (valueRangeMax > valueRangeMin) ?
	 (MIN(valueRangeMax, MAX(value, valueRangeMin))) :
	 (MIN(valueRangeMin, MAX(value, valueRangeMax)));
...

 

Hope this helps someone

JN

This topic has been closed for replies.