2023-03-24 4:57 AM
I have a TouchGFX project with some buttons used for navigating a menu. The problem is that for some reason every couple of touches is registered as a double click. So I click the touch button once, but the virtual function called by the click event is called twice. Any way to decrease the sensitivity?
I can do this in the source code, but wondering if there is a way directly in TouchGFX designer.
Solved! Go to Solution.
2023-03-28 12:52 AM
Hello @MS.12utela,
Actually, when you click a button in TouchGFX, it does not register a double-click event, but it triggers a handler with a pressed event parameter when you press the button, and when you release your finger from the button, it passes a released event to the handler.
You can get inspiration on how to decouple those 2 events from this post.
Hope that helps,
/Yoann
2023-03-28 12:52 AM
Hello @MS.12utela,
Actually, when you click a button in TouchGFX, it does not register a double-click event, but it triggers a handler with a pressed event parameter when you press the button, and when you release your finger from the button, it passes a released event to the handler.
You can get inspiration on how to decouple those 2 events from this post.
Hope that helps,
/Yoann
2023-03-30 8:51 AM
Thanks! This will help