cancel
Showing results for 
Search instead for 
Did you mean: 

Powerup problem TouchGFX with STM32F746

zekeriya
Associate II

I am working with touchGFX on the custom board with STM32F746. A 2-screen touchgfx application works without problems when debugging with cubeMXIDE. It doesn't work when I remove the STlink and powerup it. I put a heartbeat to understand that the processor is working. If I comment out the line MX_TouchGFX_Init (), then heartbeat works after powerup. I am using QUADSPI bank1 and SDRAM bank 2. FreeRtos is not used.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
zekeriya
Associate II

GCC linker script was incorrect. It should be as follows:

ExtFlashSection :

{

   *(ExtFlashSection ExtFlashSection.*)

   *(FontFlashSection FontFlashSection.*)

   *(ExtFlashSection TextFlashSection.*)

   *(.gnu.linkonce.r.*)

   . = ALIGN(0x4);

} >QUADSPI