2025-03-07 2:37 AM
I am trying to pause or stop a dynamic graph when data has scrolled to the right hand side once. I will then use a second and third etc., dynamic graph on top to display further 'screen shots' of data, to create a stack of overlays.
Is it possible to stop the graph scrolling after a given time, or number of data samples?
Thanks
Ian
Solved! Go to Solution.
2025-03-10 3:46 AM
Hello @IPrin.1 ,
The data will only scroll to the right if a new value is added.
I think that what you want is that if your graph width is 100 values, you want to show a total of 200 values so that it scroll to the right for a whole data's worth of length.
To do so you would simply have to add a number of data that is twice your graph's width (in terms of data points, not pixels).
Please find attached an example where I add 200 data points to a graph that can display 100 data points, with this amount of data, the graph scroll once to the right then stops.
I hope this helps!
If this comment answers your question, I invite you to select it as "best answer".
Regards,
2025-03-10 3:46 AM
Hello @IPrin.1 ,
The data will only scroll to the right if a new value is added.
I think that what you want is that if your graph width is 100 values, you want to show a total of 200 values so that it scroll to the right for a whole data's worth of length.
To do so you would simply have to add a number of data that is twice your graph's width (in terms of data points, not pixels).
Please find attached an example where I add 200 data points to a graph that can display 100 data points, with this amount of data, the graph scroll once to the right then stops.
I hope this helps!
If this comment answers your question, I invite you to select it as "best answer".
Regards,
2025-03-13 3:10 AM
Thanks so much, I was continuing to pass data to the graph causing it to continuously scroll. All sorted now.
2025-03-13 3:19 AM
My pleasure, I am glad I was able to help you!
Regards,