cancel
Showing results for 
Search instead for 
Did you mean: 

My touchgfx GUI is freezing though I checked signalVSync is always triggered . What could be the problem .

NKuma.3
Associate

My touchgfx GUI is freezing on my custom LCD running on STM32 MCU. I checked signalVSync is always triggered . What could be the problem ?

Here is my OSWrapper code 

using namespace touchgfx;

static xSemaphoreHandle frame_buffer_sem;

static xQueueHandle vsync_q = 0;

// Just a dummy value to insert in the VSYNC queue.

static uint8_t dummy = 0x5a;

void OSWrappers::initialize()

{

  vSemaphoreCreateBinary(frame_buffer_sem);

  // Create a queue of length 1

  vsync_q = xQueueGenericCreate(1, 1, 0);

}

void OSWrappers::takeFrameBufferSemaphore()

{

  xSemaphoreTake(frame_buffer_sem, portMAX_DELAY);

}

void OSWrappers::giveFrameBufferSemaphore()

{

  xSemaphoreGive(frame_buffer_sem);

}

void OSWrappers::tryTakeFrameBufferSemaphore()

{

  xSemaphoreTake(frame_buffer_sem, 0);

}

void OSWrappers::giveFrameBufferSemaphoreFromISR()

{

  // Since this is called from an interrupt, FreeRTOS requires special handling to trigger a

  // re-scheduling. May be applicable for other OSes as well.

  portBASE_TYPE px = pdFALSE;

  xSemaphoreGiveFromISR(frame_buffer_sem, &px);

  portEND_SWITCHING_ISR(px);

}

void OSWrappers::signalVSync()

{

  if (vsync_q)

  {

    // Since this is called from an interrupt, FreeRTOS requires special handling to trigger a

    // re-scheduling. May be applicable for other OSes as well.

    portBASE_TYPE px = pdFALSE;

    xQueueSendFromISR(vsync_q, &dummy, &px);

    portEND_SWITCHING_ISR(px);

  }

}

void OSWrappers::waitForVSync()

{

  // First make sure the queue is empty, by trying to remove an element with 0 timeout.

  xQueueReceive(vsync_q, &dummy, 0);

  // Then, wait for next VSYNC to occur.

  xQueueReceive(vsync_q, &dummy, portMAX_DELAY);

}

void OSWrappers::taskDelay(uint16_t ms)

{

  vTaskDelay(ms);

}

static portBASE_TYPE IdleTaskHook(void* p)

{

  if ((int)p) //idle task sched out

  {

    touchgfx::HAL::getInstance()->setMCUActive(true);

  }

  else //idle task sched in

  {

    touchgfx::HAL::getInstance()->setMCUActive(false);

  }

  return pdTRUE;

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0