2025-02-03 11:27 PM
I’m running into some trouble when trying to create a new application with TouchGFX Designer version 4.24.2 on the STM32N6570-DK board. After generating the code and opening the project in STM32CubeMX, I encounter a clock configuration error. It seems to resolve itself automatically, but the real issue starts when I move to STM32CubeIDE.
In STM32CubeIDE, I get an error saying the .elf file does not exist. When I try to build the project, I encounter numerous errors like "bad instruction" in tx_initialize_low_level.S.
Has anyone successfully set up a TouchGFX project for the STM32N6570-DK? Any guidance on how to resolve these issues would be greatly appreciated!
Thanks in advance for your help.
Solved! Go to Solution.
2025-02-04 12:47 AM - edited 2025-02-17 05:55 AM
Hello @TerZer ,
I have reproduced the steps you did :
I do get multiple error when building on step 4, however, I am able to fix these issues by going back to TouchGFX Designer and regenerating code between step 3 and 4.
After generating code from STM32CubeMX, you should re-generate code from TouchGFX Designer aswell.
Edit: You should also use the script mentioned in the readme to flash the board.
If this comment solves your issue I invite you to select it as "best answer".
Hope this helps!
Regards,
2025-02-04 12:47 AM - edited 2025-02-17 05:55 AM
Hello @TerZer ,
I have reproduced the steps you did :
I do get multiple error when building on step 4, however, I am able to fix these issues by going back to TouchGFX Designer and regenerating code between step 3 and 4.
After generating code from STM32CubeMX, you should re-generate code from TouchGFX Designer aswell.
Edit: You should also use the script mentioned in the readme to flash the board.
If this comment solves your issue I invite you to select it as "best answer".
Hope this helps!
Regards,
2025-02-04 02:52 AM
Hi @GaetanGodart ,
That helped, but now when I run the application, I get the following error: "Could not verify ST device! Please verify that the latest version of the GDB-server is used for connection."
Here’s the full console output:
STMicroelectronics ST-LINK GDB server. Version 7.9.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Shutting down...
Target is not responding, retrying...
Target is not responding, retrying...
Using OpenOCD:
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J15M7 (API v3) VID:PID 0483:3754
Info : Target voltage: 3.273307
Info : clock speed 8000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : [STM32N657X0HxQ.ap0] Examination succeed
Error: Failed to read memory at 0x701320d4
Error: [STM32N657X0HxQ.cpu] Examination failed
Warn : target STM32N657X0HxQ.cpu examination failed
Info : gdb port disabled
Info : starting gdb server for STM32N657X0HxQ.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: Failed to read memory at 0x701320d4
Error: Failed to read memory at 0x701320d4
Error: [STM32N657X0HxQ.cpu] Examination failed
Info : [STM32N657X0HxQ.cpu] AP write error, reset will not halt
Error: Failed to read memory at 0x701320d4
Error executing event gdb-attach on target STM32N657X0HxQ.cpu:
C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.3.0.202411041438/resources/openocd/st_scripts/gdb_helper.tcl:18: Error: TARGET: STM32N657X0HxQ.cpu - Not examined
in procedure 'gdb_attach_hook' called at file "C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.3.0.202411041438/resources/openocd/st_scripts/target/stm32n6x.cfg", line 272
in procedure 'first_gdb_attach_hook' called at file "C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.3.0.202411041438/resources/openocd/st_scripts/gdb_helper.tcl", line 18
Info : New GDB Connection: 1, Target STM32N657X0HxQ.cpu, state: reset
Error: Target STM32N657X0HxQ.cpu not examined yet, refuse gdb connection 1!
Error: attempted 'gdb' connection rejected
shutdown command invoked
It seems like the debugger cannot read memory. I also noticed that using STM32CubeProgrammer, I am unable to read memory after running the application. However, after unplugging and reinserting the cable, I can read memory again.
Any ideas on how to resolve this?
2025-02-05 02:18 AM
Hello @TerZer ,
The steps to run the STM32N6570-DK are a bit different.
Have you followed the steps mentioned in the readme file? You should not flash the board yourself but instead use scripts that we provide.
Regards,