2025-03-21 4:22 AM
Hello ,
i am using STM32h750B-dk . i took compass image (PNG file) as texture mapper and i want to rotate the compass image according to BNO055 sensor which is magnetometer. this is connected through I2C4 (for I2C4 , STmod+ is used). i have share the codes. Thank you!
#Model.cpp:
#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
#include <cstdint>
#include "stm32h7xx_hal.h"
#include <math.h>
#define BNO055_I2C_ADDR (0x28 << 1) // Shifted for STM32 HAL
#define BNO055_MAG_DATA_X_LSB_ADDR 0x0E
extern I2C_HandleTypeDef hi2c4;
Model::Model() : modelListener(0)
{
}
void Model::tick()
{
static uint32_t lastUpdateTime = 0;
uint32_t currentTime = HAL_GetTick();
if ((currentTime - lastUpdateTime) >= 1000) // Check if 1 second has passed
{
lastUpdateTime = currentTime;
if (modelListener)
{
int heading = getHeading();
modelListener->updateHeading(heading);
}
}
}
int Model::getHeading()
{
uint8_t buffer[6];
int16_t mag_data[3];
// Read magnetometer data
HAL_I2C_Mem_Read(&hi2c4, BNO055_I2C_ADDR, BNO055_MAG_DATA_X_LSB_ADDR, I2C_MEMADD_SIZE_8BIT, buffer, 6, HAL_MAX_DELAY);
// Convert to signed 16-bit values
mag_data[0] = (int16_t)((buffer[1] << 8) | buffer[0]); // X-axis
mag_data[1] = (int16_t)((buffer[3] << 8) | buffer[2]); // Y-axis
mag_data[2] = (int16_t)((buffer[5] << 8) | buffer[4]); // Z-axis
// Calculate heading angle (in degrees)
float heading = atan2((float)mag_data[1], (float)mag_data[0]) * (180.0f / 3.14159265359f);
if (heading < 0)
heading += 360; // Normalize to 0-360°
return (int)heading;
}#Screen1Presenter.cpp:
#include <gui/screen1_screen/Screen1View.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
Screen1Presenter::Screen1Presenter(Screen1View& v)
: view(v)
{
}
void Screen1Presenter::activate()
{
}
void Screen1Presenter::deactivate()
{
}
void Screen1Presenter::updateHeading(int heading)
{
view.updateCompass(heading); // Send heading to the UI for display
}#Screen1View.cpp:
#include <gui/screen1_screen/Screen1View.hpp>
Screen1View::Screen1View()
{
}
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
}
void Screen1View::tearDownScreen()
{
Screen1ViewBase::tearDownScreen();
}
void Screen1View::updateCompass(int heading)
{
float angleRadians = heading * 3.14159265359f / 180.0f;
textureMapper1.setAngles(0,0,angleRadians);
textureMapper1.invalidate();
}
Solved! Go to Solution.
2025-03-26 12:23 AM
i have update the code ..
In model.cpp , i am getting proper heading reading but in Screen1view.cpp, i am getting heading =0.
2025-03-26 12:24 AM - edited 2025-03-26 12:25 AM
am i missing something or linking between files?
2025-03-26 2:34 AM - edited 2025-03-26 2:34 AM
@Prajyot1 wrote:i have debugg the code.. i was getting same reading everytime
So your basic sensor interface was not working?
If the basic sensor interface is not working, then clearly your GUI cannot work !
The GUI cannot magically create correct data by itself !
You need to get the basic sensor interface working first !
2025-03-26 3:45 AM
Yes , i have corrected sensor code .. now it is giving proper readings.
In setHeading , i am getting proper values. but in tick() , i am not getting values
2025-03-26 3:50 AM
Please see How to insert source code - not as images.
Show the definition of currentHeading - is it volatile ?
2025-03-26 3:56 AM
yes the currentHeading is volatile
class Model
{
public:
Model();
void bind(ModelListener* listener);
void tick();
void setHeading(float heading);
protected:
ModelListener* modelListener;
volatile float currentHeading;
};
#endif
2025-03-26 4:02 AM
So what do you see in your printf output?
2025-03-26 4:07 AM
Hello @Prajyot1 ,
It is hard to follow where you are right now because you send a lot of message.
Have you fixed the error message in the comment I am responding from?
You issue could be from different reasons.
Andrew say you should check your sensor.
I think it could either be because you are not able to get the data from the model to the screenView (you have to check that your function definitions are the same so the link correctly, perhaps you can create a simple project to just test that you understand and can send data from model to view.
Another reason could be that indeed your texture mapper doesn't move, you should test that by calling a function that does that only.
Regards,
2025-03-26 4:30 AM
the values from sensor like 27.937,81 ,etc
2025-03-26 4:34 AM
@GaetanGodart yes data is not able to transfer from model to screenView.
i have rotate the texture mapper by
textureMapper1.setAngles(0.0f, 0.0f, 29.8f);
textureMapper1.invalidate();it rotate properly