Imperfect animation with TouchGSX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-07 4:59 PM
Hello,
i'm trying to execute a simple animation with TouchGFX. I'm using the Texture Mapper image, and i want to reproduce a spin of that image. As you can see in this video it was succesfully done. However, there is an extra random flashing.
I'm using the internal FLASH memory, for now. I think the problem comes from the RAM or from DMA. The latter was configured as Register to Memory, and i enables the interrupt.
While the RAM is a 16 bit (maybe too low?).
The code to create the animation is
screenViewBase.cpp
/*********************************************************************************/
/********** THIS FILE IS GENERATED BY TOUCHGFX DESIGNER, DO NOT MODIFY ***********/
/*********************************************************************************/
#include <gui_generated/screen_screen/screenViewBase.hpp>
#include <touchgfx/Color.hpp>
#include "BitmapDatabase.hpp"
screenViewBase::screenViewBase()
{
box1.setPosition(0, 0, 720, 720);
box1.setColor(touchgfx::Color::getColorFrom24BitRGB(0, 0, 0));
textureMapper1.setXY(180, 180);
textureMapper1.setBitmap(touchgfx::Bitmap(BITMAP_BACK2_ID));
textureMapper1.setWidth(360);
textureMapper1.setHeight(360);
textureMapper1.setBitmapPosition(0.000f, 0.000f);
textureMapper1.setScale(1.000f);
textureMapper1.setCameraDistance(1000.000f);
textureMapper1.setOrigo(180.000f, 180.000f, 1000.000f);
textureMapper1.setCamera(180.000f, 180.000f);
textureMapper1.updateAngles(0.000f, 0.000f, 0.000f);
textureMapper1.setRenderingAlgorithm(touchgfx::TextureMapper::NEAREST_NEIGHBOR);
add(box1);
add(textureMapper1);
}
void screenViewBase::setupScreen()
{
}
screenView.hpp
#ifndef SCREENVIEW_HPP
#define SCREENVIEW_HPP
#include <gui_generated/screen_screen/screenViewBase.hpp>
#include <gui/screen_screen/screenPresenter.hpp>
class screenView : public screenViewBase
{
public:
screenView();
virtual ~screenView() {}
virtual void setupScreen();
virtual void tearDownScreen();
virtual void handleTickEvent();
protected:
long tickCounter;
float rotation;
};
#endif // SCREENVIEW_HPP
screenView.cpp
#include <gui/screen_screen/screenView.hpp>
screenView::screenView()
{
}
void screenView::setupScreen()
{
screenViewBase::setupScreen();
tickCounter = 0;
rotation = 0;
}
void screenView::tearDownScreen()
{
screenViewBase::tearDownScreen();
}
void screenView::handleTickEvent()
{
tickCounter++;
if(tickCounter % 30 == 0)
{
rotation += 0.1;
textureMapper1.updateAngles(0.000f, rotation, 0.000f);
}
}
I hope you can help me.
Alberto
Solved! Go to Solution.
- Labels:
-
STM32F7 Series
-
TouchGFX
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-08 6:12 AM
I solved this problem scaling the LCD-TFT frequency from 48MHz to 25MHz.
However, i noticed a remerkable lag between frames, expecially when the image is full displayed. I think this is a rendering problem now. Is there a way to get this faster?
I have an STM32F767IGT microcontroller, with a 720x720 display at 18 bits (scaled to 16 bits by TouchGFX). As i said in the previous post i'm using DMA2D register to memory but i don't know if i need some extra configurations to improve performances.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-08 6:12 AM
I solved this problem scaling the LCD-TFT frequency from 48MHz to 25MHz.
However, i noticed a remerkable lag between frames, expecially when the image is full displayed. I think this is a rendering problem now. Is there a way to get this faster?
I have an STM32F767IGT microcontroller, with a 720x720 display at 18 bits (scaled to 16 bits by TouchGFX). As i said in the previous post i'm using DMA2D register to memory but i don't know if i need some extra configurations to improve performances.