cancel
Showing results for 
Search instead for 
Did you mean: 

Im new to CubeIDE. When Setting up RCC (Low speed clock) to crystal resonator and adding clock and calendar in RTC, it says the HAL_RTC_Init is not defined.. how can I fix this?

Amaresh
Associate III

0693W00000KauhSQAR.png

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Amaresh
Associate III

BTW this ioc is setup by touch gfx. When I open an ide project directly and do the same thing it doesn't give the error.

The Console tab has the exact error message. The Problems tab is the IDE’s “helpful�? way of reordering things, which is less than helpful.
The full output from the console tab would show the actual issue. Solving it is another thing. Looks like the RTC file isnt being compiled.
If you feel a post has answered your question, please click "Accept as Solution".
Amaresh
Associate III
make -j8 all 
arm-none-eabi-g++ -o "STM32F469I-DISCO.elf" @"objects.list"  -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m4 -T"C:\TouchGFXProjects\TestTimeandDate_3\STM32CubeIDE\STM32F469NIHX_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32F469I-DISCO.map" -Wl,--gc-sections -static -LC:/git/STM32F469-dk/stm32f469i_disco/STM32F469I-DISCO/Middlewares/ST/touchgfx/lib/core/cortex_m4f/gcc -LC:/git/stm32f469i_disco/STM32F469I-DISCO/Middlewares/ST/touchgfx/lib/core/cortex_m4f/gcc -LC:/TouchGFXProjects/TestTimeandDate_3/Middlewares/ST/touchgfx/lib/core/cortex_m4f/gcc --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: ./Application/User/main.o: in function `MX_RTC_Init':
C:/TouchGFXProjects/TestTimeandDate_3/Core/Src/main.c:623: undefined reference to `HAL_RTC_Init'
c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: C:/TouchGFXProjects/TestTimeandDate_3/Core/Src/main.c:639: undefined reference to `HAL_RTC_SetTime'
c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: C:/TouchGFXProjects/TestTimeandDate_3/Core/Src/main.c:648: undefined reference to `HAL_RTC_SetDate'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:88: STM32F469I-DISCO.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
 
10:04:18 Build Failed. 5 errors, 0 warnings. (took 1s.898ms)
 

Here is the console error message

Yes I think the RTC isn't being compiled for some reason when the project is opened through touchgfx