cancel
Showing results for 
Search instead for 
Did you mean: 

I just installed Touchgfx for the first time and I wanted to check out the demos, but it seems like there are no demos or examples at all. Where do i get the demos i saw on the website?

RMang.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Yoann KLEIN
ST Employee

Hello @RMang.1​ ,

The demos and examples are in TouchGFXDesigner :

  • Open TouchGFXDesigner.
  • On the left menu of TGFXDesigner you will see the tabs "Examples" and "Demos".
  • Select an example or a demo.
  • Select a Board Setup if you want to run this example on a specific board.
  • Click on "Create", on the bottom right corner of the window, to create a project.

Hope that this helped you,

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX
GWowe.1
Associate II

Hello,

I suppose the problem you observed maybe caused by a problem with the internet connection which loads the examples & demos. Anyway, if your problem is not resolved by the actions

proposed by Yoann. You should have an eye on the answers to be expected on my post of 2nd march.

Greetings

Gerhard

Hello,

Like you said, there could also be an issue with the internet connection, which is of course required to load the examples and the demos, but @RMang.1​ didn't mention that kind of problem in his post.

I also answered about possible causes and solutions to fix that connection issue, on your post @GWowe.1​ .

Thank you @Community member​ for providing the link.

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX