cancel
Showing results for 
Search instead for 
Did you mean: 

i'm using STM32H747XI and STM32CubeMX , TouchGFX. i did generated code using STM32CubeMX and TouchGFX . But code is not compiled at IAR 9.10.2. what can i do solve this?? Best regard. error is below..

ysuh.1
Associate

0693W00000Bd7BIQAZ.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amira
Associate III

Hello @ysuh.1​ 

STM32H7 package is compatible with V8.30.1 + ST-LINKV3 as mentioned in firmware release notes. IAR 9.X is not yet supported.

So, I think you have to switch the IAR version to 8.30.1 (and below).

PS: Once your question is answered, please click on "Select as Best" for the comment containing the answer to your initial question.

Regards,

Amira

View solution in original post

1 REPLY 1
Amira
Associate III

Hello @ysuh.1​ 

STM32H7 package is compatible with V8.30.1 + ST-LINKV3 as mentioned in firmware release notes. IAR 9.X is not yet supported.

So, I think you have to switch the IAR version to 8.30.1 (and below).

PS: Once your question is answered, please click on "Select as Best" for the comment containing the answer to your initial question.

Regards,

Amira