2019-11-14 2:43 AM
Screen3View.hpp (Where the keyboard should be visible)
#ifndef SCREEN3VIEW_HPP
#define SCREEN3VIEW_HPP
#include <gui_generated/screen3_screen/Screen3ViewBase.hpp>
#include <gui/screen3_screen/Screen3Presenter.hpp>
#include <gui_generated/screen3_screen/Screen3ViewBase.hpp>
#include <gui/screen3_screen/Screen3Presenter.hpp>
#include <gui/common/CustomKeyboard.hpp>
#include <touchgfx/widgets/ButtonWithLabel.hpp>
class Screen3View : public Screen3ViewBase
{
public:
Screen3View();
virtual ~Screen3View() {}
virtual void setupScreen();
virtual void tearDownScreen();
protected:
CustomKeyboard keyboard;
};
#endif // SCREEN3VIEW_HPP```
Screen3View.cpp
Screen3View::Screen3View()
{
keyboard.setPosition(16, 16, 400, 240);
add(keyboard);
}Screen4View.hpp (where the keyboard should **not** be visible)
#ifndef SCREEN4VIEW_HPP
#define SCREEN4VIEW_HPP
#include <gui_generated/screen4_screen/Screen4ViewBase.hpp>
#include <gui/screen4_screen/Screen4Presenter.hpp>
class Screen4View : public Screen4ViewBase
{
public:
Screen4View();
virtual ~Screen4View() {}
virtual void setupScreen();
virtual void tearDownScreen();
protected:
};
#endif // SCREEN4VIEW_HPP
```
Screen4View.cpp
Screen4View::Screen4View()
{
}
all other.cpp of the TouchGFX files "say" the exact same thing.
Just Screen 3 should have this keyboard, and not Screen 4 too.
So if anybody has an idea why it is like that please answer. :)
Thank you very much.
2019-11-14 4:14 AM
Hi,
Am i to understand that Screen 4 is just an empty canvas?
Imagine what happens if you "switch to a screen" that renders nothing - What would you expect to be in the framebuffer? (Hint: A Blank canvas is like looking out of your window).
/Martin