cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STM32F750Z8T6 for a product called Emergency Talk-back, which will be used in Railway. There is Touch TFT LCD ( 18bit) with RBG interface connected with the micro controlle. The TFT LCD prt no is WF70A6TIAGDNG0 (winstar make), it is compatible

small.11
Associate
 
1 REPLY 1
TDK
Guru

> it is compatible

Was this meant to be the question?

Should be compatible in RGB666 mode. Look at the signal in the datasheet and ensure you know where you connect them on the STM32. Do a pinout check first.

If you feel a post has answered your question, please click "Accept as Solution".